2019-07-04 4:01 PM
Hi,
I have a SensorTile.box from ST. But unfortunately there is no board schematics in the product resources part! I appreciate if some one help and let me know about it.
Kind regards
Solved! Go to Solution.
2019-08-02 4:48 AM
Glad to inform you that the SensorTile.box block diagram and schematics are now available online --> link
Regards
2019-07-05 12:28 AM
Hi @Am , the schematics will be soon available on st.com (I hope in a couple of weeks). It's not available by now due to some cosmetic changes. Regards
2019-07-23 11:10 PM
Hi
Any update on this?
thanks!
2019-07-24 5:05 AM
HI @RafaelJoseph , unfortunately not yet, but should be soon ready. My two-weeks hypothesis was too optimistic, cause I did't take into account the vacation period. Sorry for the delay. Regards
2019-08-02 4:48 AM
Glad to inform you that the SensorTile.box block diagram and schematics are now available online --> link
Regards
2019-08-02 5:00 AM
Thanks for the update!
2020-06-04 1:33 AM
I was wondering, if the SensorTile.box block diagram and schematics (link) are correct. If I am not mistaken it should contain a LSM6DSOX sensor, which is connected through SPI1. (My statements are based on the code generated by Algobuilder.)
Best regards,
Attila
2020-06-04 1:51 AM
Hi @AKato.1 , you are right, the IMU sensor on the ST.box is a LSM6DSOX and not a LSM6DSO. There is a mistake on the schematic... Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.