2016-02-17 5:36 AM
We have a LIS3DH accelerometer that have ended up in a latch-up state. The output data is -205/-1149/-4759 (X/Y/Z in mg). When performing the self test, the absolute difference between the 2 samples are 7/6/3 (X/Y/Z in mg) which is well below the min limit (> 60mg). Is there any way to recover from this? Do I have to make the accelerometer powerless?
#latch-up2016-02-17 6:15 AM
I use LSM303D and sometime falling in an state of maximum data out on all axis.
Power down, reset ecc. not wake the accelerometer.The one solution is a strong shock/crash several times and the accelerometer starts running again.This is really a problem ... and we do not know how to solve it.It seems a problem similar to yours.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.