cancel
Showing results for 
Search instead for 
Did you mean: 

Run HS Datalog from Raspberry Pi 3B to Collect Data from STEVAL-STWINKT1B

digidhamu
Associate III

As per the Release Notes (v2.4.0 / 5-Nov-2021) for HS DataLog CLI example, I could see executable and libs are present under directory Utilities/cli_example for Raspberry Pi 3B. I have also exported and set the shared library path using command.

export LD_LIBRARY_PATH=<Utilities/cli_example/bin>

But when I execute below command

./bin/cli_example_rpi3b -f ../STWIN_config_examples/DeviceConfig.json -t 100

I am getting following error error.

./cli_example_rpi3b: error while loading shared libraries: libhs_datalog.so: wrong ELF class: ELFCLASS64

Could you please advise whether I am doing anything wrong?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
SimonePradolini
ST Employee

Hi @digidhamu​,

To overcome any kind of configuration issues, we will provide a configuration script for linux and raspberry in the FP-SNS-DATALOG1 v1.4.0.

This new version will be available by the end of July/first days of August.

You will just lunch the raspberry_setup/setup_rpi3b.sh script, and then everything should work properly.

I suggest you to update the CLI once available.

In your use case, you are loading the entire /bin folder, that contains both Linux and Raspberry .so version.

The Linux one (libhs_datalog.so) can't work on Raspberry and maybe that's the reason for the error.

Move libhs_datalog.so into another folder and launch newly the script.

Do you still have the same error?

Best regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.