cancel
Showing results for 
Search instead for 
Did you mean: 

Response time of LPS sensor

ljm
Associate III

Hello,

 "1/ODR (1 à 200 HZ)" is it the response time of the sensor ?

Thank you 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @ljm ,

What do you mean with "response time"? 

If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Federica Bossi
ST Employee

Hi @ljm ,

What do you mean with "response time"? 

If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Federica Bossi  

I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is  ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the range -15 to 65°C?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.