2020-01-14 1:33 AM
Dear STM Sensor specialist ..
I have a customer who up until now have used 1 LSM6DSLTR on his powerboard.
Now they designed a new powerboard with 2 pcs LSM6DSLTR and now they are facing some read out issues.
Electrically it is a copy of the old design with the same I/O interface to our MCU.
But on the new new Powerboard, they are unfortunately experiencing some errors where the data from LSM6DSLTR periodically stops or or fall out ..
They sometimes see 10 mistakes in one minute and at other times no error in 3 hours.
We see the error randomly on both of the LSM6DSLTR, sometimes on the number 1sensor and sometimes on number 2, so it seems not to be limited to the specific location on the board but more like cross talking or timing issues ??
The question is, whether ST has some good suggestions on what might be the reason, is there special things to be aware of ? also in relation to handling or soldering processes at the EMS. do you know have any issue Experiences or special "behaviors" by the IC?
And of course how to proceed in the matter?
With best regards
Kenny Teist
Rutronik Electronics Denmark ApS
2020-01-17 6:25 AM
Hi @KTeis.1571 , how are the two sensors connected to the MCU? Two different I2C/SPI lines or are they sharing e.g. the same SPI (SCLK, MISO, MOSI) lines except from the CS line? And which are the Vdd and the VddIO values? Could it be possible for you ro share the relevant part of the schematic of your customer's board? Regards
2020-01-21 1:01 AM
2020-01-21 2:11 AM
2020-01-22 8:17 AM
Hi Kenny, which is the interested customer? My email address is eleon.borlini@st.com, but I would suggest you to the standard support channel, that is the online support at this link selecting the Sales and representatives of customer's region. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.