2016-10-04 6:22 AM
Hi.
I'm testing LSM303AGR. If I put my sensor module on the my desk, Z value of accelerometer's output is about 1400 LSB. I'm using high resolution mode(12bit) and 16g range. If I calculate this value as mg unit, the output value is calculated as 16,408mg. I expected the output value about 1000mg(Gravity), but the result is quite different. Could you give me some comment about the resolution of this sensor? #lsm303agr #resolution.2017-03-16 7:38 AM
Are you sure about those values? How do you calculate mg? What are the actual LSB and MSB register values?
16408 >> 4 would amount to 1025mg so something feels fishy here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.