2015-05-12 3:02 AM
Hi ,
we are using LIS331DLH accelerometer for our application.
I have some doubts regarding acceleration values.
1) I don't get any horizontal acceleration for below configuration.
Threshold: 500mg.
Interrupt 1 is enabled
INT1_CFG = 0X2A (XH, YH and ZH enabled)
2) I get horizontal acceleration when i enable 6D direction movement. But it produce continuous interrupt for small movement with below configuration.
Threshold: 1000mg
Interrupt 1 is enabled
INT1_CFG = 0X6A (XH, YH and ZH enabled and 6D direction movement)
3) From the datasheet in steady state, sensor has x =0g, y = 0g and z = 1g. If I set threshold 500mg and enabled acceleration in z axis, will it produce continuous interrupt?
Because Already the acceleration in z direction 1000mg (1g).
Thanks in advance
Regards,
Keerthi G.
#acceleration #lis331dlh-sensorWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.