2016-05-26 12:00 PM
I would like to use VL6180X more like a conventional proximity sensor where an output pin is active a target is within range, and the output is inactive when the target is outside the specified range. I don't see a way to do this without having an interrupt service.
Is there a way?Will the VL52L0X have this ability?2016-05-31 7:46 AM
I see the datasheet is available for the V53L0X. Section 2.7 indicates the only way to find the status of the over, under, or range window is by polling over the I2C bus, or by an interrupt, which also requires an I2C response.
What would be useful to me is to configure the GPIO1 pin to show the status of the last measurement (over, under or in window range). Who would know if this feature will be added?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.