2022-05-29 11:21 PM
Hello,
lsm6dsox is configured to 1667Hz ODR.
And I measured 'data ready interrupt' interval of 9 sensors.
It was between 1629.69 and 1683.57Hz.
I wonder if there is acceptable deviation criteria?
Solved! Go to Solution.
2022-06-03 6:39 AM
Hi @Community member ,
Please consider that the actual ODR frequency is a typical value (typ on the datasheet), that can slightly vary from the nominal value.
In particular, in HP mode the variation among samples can be +-1% typ, while in NM can be about +-2% (data on 100 characterization samples).
If you want to synchronize on ODR, you have to measure it sample by sample with the DRDY method, as you already correctly did.
-Eleon
2022-06-03 6:39 AM
Hi @Community member ,
Please consider that the actual ODR frequency is a typical value (typ on the datasheet), that can slightly vary from the nominal value.
In particular, in HP mode the variation among samples can be +-1% typ, while in NM can be about +-2% (data on 100 characterization samples).
If you want to synchronize on ODR, you have to measure it sample by sample with the DRDY method, as you already correctly did.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.