2018-05-28 5:39 AM
I have an STM32F303 Discovery and I want to use the I2C bus to receive the x,y,z data from an accelerometer MPU6050. Does anyone have source code for this? The problem is that the address of the buffers (i2cBuff) are 0, and the Xaccel, Yaccel, Zaccel too.
Here is my code:
&sharpinclude 'main.h' &sharpinclude 'stm32f3xx_hal.h'I2C_HandleTypeDef hi2c1; &sharpdefine mpu6050Address 0xD0 uint8_t i2cBuf[8];uint16_t ax,ay,az;float Xaccel,Yaccel,Zaccel;int main(void) { //HAL Initialise HAL_Init(); //Config functions GPIO_Config(); I2C_Config(); //1. Scan the I2C addresses for(uint8_t i=0; i<255; i++) { if(HAL_I2C_IsDeviceReady(&hi2c1, i, 1, 10) == HAL_OK) { HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12); break; } } //2. I2C Write example //a) Set accelerometer range (reg28) i2cBuf[0] = 28; //Register address: Accelerometer config 1 i2cBuf[1] = 0x08; //Data to write, +-8g range HAL_I2C_Master_Transmit(&hi2c1, mpu6050Address, i2cBuf, 2, 10); //3. I2C Read example //Request to read from a register (reg28) i2cBuf[0] = 28; //Register address: Accelerometer config 1 HAL_I2C_Master_Transmit(&hi2c1, mpu6050Address, i2cBuf, 1, 10); //Read data i2cBuf[1] = 0x00; HAL_I2C_Master_Receive(&hi2c1, mpu6050Address|0x01, &i2cBuf[1], 1, 10); while(1) { //4. Read accelerometer data HAL_I2C_Mem_Read(&hi2c1, mpu6050Address, 0x3B, I2C_MEMADD_SIZE_8BIT, &i2cBuf[1], 6, 10); ax = -(i2cBuf[1]<<8 | i2cBuf[2]); ay = -(i2cBuf[3]<<8 | i2cBuf[4]); az = (i2cBuf[5]<<8 | i2cBuf[6]); Xaccel = ax/8192.0; Yaccel = ay/8192.0; Zaccel = az/8192.0; HAL_Delay(50); } }#accelerometer #i2c #mpu6050 #stm32f32018-06-26 7:54 AM
Hello toufik!
I had the same problem and I fix it by putting a greater value in the timeout of the read() and write() operations because 10ms could be very fast for a I2C communication.
I hope it could help
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.