2022-01-06 6:08 AM
Hello,
It seems that the library MotionMC_CM7F_wc32_ot_hard.a is missing the called function, here the error :
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ../Middlewares/ST/STM32_MotionMC_Library/Lib\MotionMC_CM7F_wc32_ot_hard.a(motion_mc.o): in function `MotionMC_Initialize':
motion_mc.c:(.text.MotionMC_Initialize+0xde): undefined reference to `MotionMC_SaveCalInNVM'
c:\st\stm32cubeide_1.6.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: motion_mc.c:(.text.MotionMC_Initialize+0x1fc): undefined reference to `MotionMC_LoadCalFromNVM'
I'm just doing like the example, I erased and reinstalled MEMS and this library at the previous version but nothing changes, can you help me ?
Here the call :
#define VERSION_STR_LENGTH 35
#define SAMPLE_TIME 20
/* Magnetometer calibration API initialization function */
MotionMC_Initialize(SAMPLE_TIME, 1);
Solved! Go to Solution.
2022-01-06 6:28 AM
Please add following function in your code.
// NOTE: Must be implemented for each platform separately, because its implementation
// is platform dependent. No need to call this function, library call this
// function automatically.
/**
* @brief Load the calibration parameters from storage
* @param dataSize size of data
* @param data pointer to data
* @retval Will return 0 the if it is success and 1 if it is failure
*/
char MotionMC_LoadCalFromNVM(unsigned short int datasize, unsigned int *data)
{
return 1; /* FAILURE: Read from NVM not implemented. */
}
// NOTE: Must be implemented for each platform separately, because its implementation
// is platform dependent. No need to call this function, library call this
// function automatically.
/**
* @brief Save the calibration parameters in storage
* @param dataSize size of data
* @param data pointer to data
* @retval Will return 0 the if it is success and 1 if it is failure
*/
char MotionMC_SaveCalInNVM(unsigned short int datasize, unsigned int *data)
{
return 1; /* FAILURE: Write to NVM not implemented. */
}
2022-01-06 6:28 AM
Please add following function in your code.
// NOTE: Must be implemented for each platform separately, because its implementation
// is platform dependent. No need to call this function, library call this
// function automatically.
/**
* @brief Load the calibration parameters from storage
* @param dataSize size of data
* @param data pointer to data
* @retval Will return 0 the if it is success and 1 if it is failure
*/
char MotionMC_LoadCalFromNVM(unsigned short int datasize, unsigned int *data)
{
return 1; /* FAILURE: Read from NVM not implemented. */
}
// NOTE: Must be implemented for each platform separately, because its implementation
// is platform dependent. No need to call this function, library call this
// function automatically.
/**
* @brief Save the calibration parameters in storage
* @param dataSize size of data
* @param data pointer to data
* @retval Will return 0 the if it is success and 1 if it is failure
*/
char MotionMC_SaveCalInNVM(unsigned short int datasize, unsigned int *data)
{
return 1; /* FAILURE: Write to NVM not implemented. */
}
2022-01-06 7:49 AM
Thank you, it works.
2025-01-23 2:47 AM
Hello,
Where did you implement these functions in your code to make it work?
Thanks,
2025-10-07 10:18 AM
Hello
I have the same question as Melodi, that is where should I implement such two functions?
I have tried some method, but they do not work. First, I implement these two functions in a sandbox in main.c, it does not word. Then I create a source file motion_ac.c in the same fold as motion_ac.h, and implement these two functions in motion_ac.c and declare function prototype in motion_ac.h, but it does not work either.
So, where should I implement such two functions?
Thanks
2025-10-07 10:42 AM
I have solved this problem.
These two functions should be implemented in a sandbox in main.c,and their function prototypes should be declared in main.h.
I previouly treated them as weak functions without declared prototypes, which lead to compile errors.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.