cancel
Showing results for 
Search instead for 
Did you mean: 

MOTENV1_ENABLE_PRINTF

Dilbert K
Senior
Posted on July 26, 2017 at 23:26

HW : STM32L476RG-SensorTile

SW : SW4STM32

Tried to enable the debug print through USB.

I was using the BlueMicrosystem2_V2.2.0.  Enable  #define OSX_BMS_ENABLE_PRINTF and rebuild code will work.

Can see all the print out.

Recently got the new STM32CubeFunctionPack_MOTENV1_V3.0.0.

Followed the instruction in main.c to rebuild with #define  MOTENV1_ENABLE_PRINTF 

But the ST Virtual COM port not even showing up in PC device manager

Is there additional work need to be done ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Dilbert K
Senior
Posted on July 27, 2017 at 00:47

OK, found the problem, this was old problem for using AC6.

As #elif will not work for just #define, need to change all the build options define in project to =1

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.