cancel
Showing results for 
Search instead for 
Did you mean: 

BlueMicrosystem2 with Android Apps disconnect

Dilbert K
Senior
Posted on June 21, 2017 at 22:20

I am using the BlueNRG-MS on SensorTile and loaded the BlueMicrosystem2 firmware.

When connecting/disconnecting with ST BlueMS App using iPhone.  Everything is OK.

When testing the same with Android phone (Android 5.0.1), it can connect and communicate.

However, after exit the 

ST BlueMS App and try to Scan for device again.  The device cannot be found anymore.

Checking the firmware, the status indicate device still in 'connected' state.

Should there be a timeout for this ?

The only way to have device advertise again is 'reset' firmware

Thanks for advice.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Giovanni Visentini
Associate II
Posted on June 22, 2017 at 12:04

Hi Dilbert,

I need some information to reproduce the problem.

- Does it always happens or only after that you run some specific demos?

- 'exit the ST BlueMS' means that you put it on background or you you put on

background

+ delete it from the app stack?

- are you using the Bluemicrosytem2 v2.2?

Thanks

Giovanni

Posted on June 22, 2017 at 16:21

Hi Giovanni,

- I tested number of times and it happened every try.  Wonder this is Android V5.0.1 issue as it is pretty old version.

'exit the ST BlueMS' means I try to disconnect the device & Apps.  In the Apps, I simply return to 'Start discovering' page.

- Yes, I am using 

Bluemicrosytem2 v2.2

Posted on June 29, 2017 at 17:58

Hi Dilbert,

It may be a problem related with a strange combination of Android version + mobile model.. could you try with a different mobile/android version?

Sorry but with my test devices I never see a problem like that.. 

Best Regards

Giovanni

Posted on July 26, 2017 at 23:14

Yes, got a different version Android phone (V6.x.x) and the issue not happening. 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.