2013-10-14 6:04 AM
I have the STEVAL-MKI109V2 with the MKI135V1 accelerometer module. I've installed the Unico eval software v3.0.0.0. The COM port matches. There are no errors. I'm on Win7/64.
There is no data.What am I missing?Thanks! #unico2013-10-21 6:20 AM
*bump*
Anyone have a suggestion? I just need to show my boss that this device works, and then we can add a motion detect feature to our product.Thanks.2013-10-22 5:41 AM
2013-10-22 10:21 AM
Hello Thiago,
Thanks for responding. Whenever I change the setting away from Power Down Mode (Eg Normal 25Hz), nothing happens. If I switch to the Data screen, and then back to the Settings screen, it reverts to Power Down Mode.It acts like there is no communications at all, but there are no errors. Changing screens take a very long time (10-20 secs), which suggests a communications timeout.The Windows Device Manager says that the Virtual Comm is working properly.What is my next step?2013-10-28 6:01 AM
Hi Thiago,
Any update?Thanks.2013-11-18 4:46 AM
Hello Dan,
In order to better respond to your question, would you please send me a screenshot of the problem that you are facing? Specially of the settings tab of the Unico Gui. I believe there must be a connection problem between the computer and the sensor that you are trying to evaluate. Thank you, Thiago Reis2013-11-18 2:00 PM
Hi Thiago,
I was able to get some assistance from internal support through my sales rep.It seems that my version requires the latest Unico (v3.0.0.1) and a firmware upgrade.I hope to have a new demo kit by the end of the week.Dan2013-11-19 6:16 AM
Hello Dan,
I am glad that you have found a solution for the issue you were facing. Please do not hesitate on posting any other questions or topics that you would like to discuss. Thank you very much, Thiago ReisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.