2013-10-09 5:52 PM
The RDY is used to indicate a new data is available. The problem is that the ODR can not greater than 160Hz,otherwise after a period of time of dataoutput,the RDY goes low,and the value of STATUS_REG is changed to 0x77(why??). The initial code follows:
Write_Command(CTRL_REG1, 0xE7); Delay_Time(10); Write_Command(CTRL_REG2, 0x14); Delay_Time(10); Write_Command(CTRL_REG1, 0xE7); Write_Command(CTRL_REG3, 0x18); Delay_Time(10); Write_Command(CTRL_REG2, 0x44); Delay_Time(10); #lis3lv02dq2013-11-18 8:00 AM
Hello Kong,
In order to better answer your question, could you please send me the registers setup of your sensor? In specialCTRL_REG2 (21h).
Thank you very much, Thiago ReisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.