2014-08-24 1:44 AM
Hi, I'm trying to understand the readings I got for a LSM9DS0 on my board. If I hold the board on my desk, according to the datasheet I should read a negative value for the Z-AXIS, because Z-AXIS vector points up, instead I read a positive 1g value.
The same happens with the other two axes. Are all the readings inverted? Or am I wrong with something?2015-05-07 11:32 PM
I have asked same thing, but this is a useless forum.
2015-07-29 2:13 AM
Hello,
are you using the linux driver? If yes you must play with the init data: #if defined(CONFIG_LSM9DS0) static struct lsm9ds0_acc_platform_data lsm9ds0_acc_data = { .fs_range = LSM9DS0_ACC_FS_2G, .rot_matrix = { {1, 0, 0}, {0, 1, 0}, {0, 0, 1}, }, .poll_interval = 500, .min_interval = LSM9DS0_ACC_MIN_POLL_PERIOD_MS, .aa_filter_bandwidth = ANTI_ALIASING_773, .gpio_int1 = 149, .gpio_int2 = 151, }; static struct lsm9ds0_mag_platform_data lsm9ds0_mag_data = { .poll_interval = 500, .min_interval = LSM9DS0_MAG_MIN_POLL_PERIOD_MS, .fs_range = LSM9DS0_MAG_FS_2G, .rot_matrix = { {1, 0, 0}, {0, 1, 0}, {0, 0, 1}, }, }; static struct lsm9ds0_gyr_platform_data lsm9ds0_gyr_data = { .poll_interval = 500, .min_interval = LSM9DS0_GYR_MIN_POLL_PERIOD_MS, /* 2ms */ .fs_range = LSM9DS0_GYR_FS_250DPS, /* gpio ports for interrupt pads */ .gpio_int1 = 152, .gpio_int2 = 153, /* int for fifo */ .axis_map_x = 0, .axis_map_y = 1, .axis_map_z = 2, .negate_x = 0, .negate_y = 0, .negate_z = 0, }; static struct lsm9ds0_main_platform_data lsm9ds0_acc_mag_data = { .pdata_acc = &lsm9ds0_acc_data, .pdata_mag = &lsm9ds0_mag_data, }; #endif /* CONFIG_LSM9DS0 */2015-07-29 6:32 AM
I think you've misunderstood something.
The accelerometer measures acceleration relative to the free fall reference frame. That is, if the accelerometer had been in free fall, you would measure zero acceleration. Relative to this, the accelerometer is accelerating upwards at a rate of 1 g when it is flat on your desk.. Therefore you will read +1 g.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.