2021-03-01 9:13 AM
Is the only difference between the two that LSM6DSOX has the machine-learning core (MLC)?
In other words, are the 2 parts interchangeable when the MLC is not used?
Solved! Go to Solution.
2021-03-02 12:01 AM
Hi @Andrew Neil ,
basically yes, if you don't mind the MLC feature the two part numbers are interchangeable.
-Eleon
2021-03-02 12:01 AM
Hi @Andrew Neil ,
basically yes, if you don't mind the MLC feature the two part numbers are interchangeable.
-Eleon
2021-03-02 2:39 AM
Great - thanks.
So, if you have an existing design with LSM6DSO, you could just drop-in an LSM6DSOX to gain the MLC features?
In fact, I have an X-NUCLEO-IKS01A3 (with LSM6DSO) - so I could use that to get started, and just add MLC stuff later when/if I move to LSM6DSOX ?
2021-03-02 3:05 AM
Yes, that's right, you can take a STEVAL-MKI197V1 and plug it on the DIL24 connector of the X-NUCLEO-IKS01A3 (without un-soldering previous LSM6DSO).
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.