cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSO SPI Bug for high volume project

ZarvanM
Associate

Using the LSM6 over SPI with the RP2040 Microcontroller for a mission-critical project (flight controller for UAVs).

The SPI works well. Well in theory. In practice, 1 in every 20-100 reads returns corrupt SPI data (WHOAMI reads as 0x68/0x58). This issue is somewhat reduced when moving the sensor (worst when still) and when adding decoupling capacitors (reduces corruption dramatically).

The project itself is ultra high volume (10k+ units), and we have already invested a very large amount of time and resources into testing.

2 REPLIES 2
TDK
Super User

> In practice, 1 in every 20-100 reads returns corrupt SPI data (WHOAMI reads as 0x68/0x58).

> we have already invested a very large amount of time and resources into testing.

These statements are somewhat at odds. A 1-5% failure rate should be pretty easy to check.

 

No magic bullet here. Some things that can help:

  • Lower clock speed and/or slower edges.
  • Better shielding from EMI.
  • Terminating resistor on SPI line with or without controlled impedance.
  • LVDS or similar differential transceivers at each end.
  • Decoupling capacitors.
  • Reduced signal/wire length.
  • Better grounding (avoid loops).

 

A UAV will have higher EMI than a normal application. Consider decoupling capacitors a must rather than a recommendation.

If you feel a post has answered your question, please click "Accept as Solution".

Hi!

Thanks for the reply.

Yes, we have followed best practices, and the failure occurs on with bench testing, not yet on a UAV.

The 1-5% failure rate is influenced by:

1. Whether the IMU is untouched

2. Adding lots of electrolytics at input

3. Changing SPI speed (lower sometimes causes MORE problems)

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.