2022-05-02 10:56 PM
Hello,
I'm in the evaluation stage of LSM6DSO sensor. I've got a SensorTile.Box module and running DataLogExtended.bin firmware and I use Unicleo-GUI to read sensors' data. I'm expecting to get 0 values for the gyro outputs if the module is stationary but instead, I'm getting -1100 on the Y putout and some other values on the other axis. Attached is the screenshot of the Unicleo-GUI graph.
Do I need to calibrate the sensor before start reading the values?
If Yes, is there any way to do it via the GUI?
Regard
K
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.