2016-11-23 2:58 AM
Hi,
The typical supply voltage for the LSM6DS33 is 1.8V and the maximum limit is 3.6V. Is it fine if a supply voltage of 3.3V is continously provided to the device?Regards,Prachi #lsm6ds332016-12-01 3:14 AM
Hello,
Yes, since the LSM6DS33 analog supply voltage range is from 1.71 V to 3.6 V it is more than fine if a 3.3V supply voltage is continuously provided to the device.Thank you and best regards,PetrWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.