cancel
Showing results for 
Search instead for 
Did you mean: 

lsm6ds3 SPI code

suresh
Associate II
Posted on July 27, 2016 at 23:17

Hello, We are using lsm6ds3 sensor by connecting to STM32F103 controller through I2C communication. Over I2C to read both X and G Raw data taking around 800uSeconds over 400K speed.

In one of my new project, needed both X&G raw values for every millisecond.

For fast reading, thinking to use SPI communication instead of I2C communication. Provided examples with in X-CUBE-MEMS1 are based off I2C, is there example any examples for SPI connection?

Regards,

Jim

#lsm6ds3 #stm32f10x #4-wired-spi
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Petr S
ST Employee
Posted on July 29, 2016 at 09:11

Hello Tim,

Unfortunatelly X-CUBE-MEMS1 package uses the IKS01A1 MEMS Shield expansion board which does not support SPI at all so therefore there is no sample code for SPI.

Best regards,

Petr

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.