2017-01-23 4:03 AM
Hi,
I am using STEVAL-MKI160V1 evaluation module of LSM6DS3 in arduino platform with 8g scale. When I turn this 1g to -1g , it suddenly fall to 89 , 86 , 89.......etc , from 4173
(1g reading, that i got)
with a tilt of less than 5 degree from initial position , ie the g value varies not sinusoidally. it gives some valid values in some other positions between a rotation of 1g to -1g, and again falls to invalid values mentioned above, Due to this my Madgewick filter give me , error output. Attaching my codes , Please help to solve this problem2017-01-24 2:14 AM
Hello
I have moved your thread to the
‌ where someone should be able to help you.Thanks
Oli
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.