2016-07-25 9:19 PM
Should my program get 1000 mg when F3 Discovery Board is in steady state on a horizontal surface?
Measurement range = [-2g;+2g]; Linear Axeleration Sensitivity = 1mg/LSB; High Resolution Mode I get 15344 mg (0x3BF0) and -16912 mg (0xBDFO) when the board is upside-down.2016-08-01 9:35 AM
The output of the accelerometer sensor is 12-bit left adjusted. You have to divide the sensor output value by 16, then you will get correct value in [mg] unit.
Best regardsMiroslavWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.