cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303AGR I2C

portatil
Associate
Posted on October 11, 2016 at 12:21

I need connect 3 LSM303AGR in the same I2C bus. Is It possible?

How do I change the I2C Address?  

#lsm303agr #i2c
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on October 11, 2016 at 15:24

Unfortunately it is not possible to connect more than one LSM303AGR sensor on the same I2C bus, because the I2C address is fixed.

The solution could be to use more I2C buses or connect the sensors on SPI bus and distinguish them by chip select (CS) signal.

Best regards

Miroslav

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.