2019-07-22 10:49 AM
Hi, I am using the LPS22HB and noticed it was reading significantly off after installation. The datasheet and applications notes really don't address this and a good way to correct for it. Could you look at enhancing your application notes or technical notes for this specific issue and address how the factory calibrates and what a user *should* do to restore accuracy?
Thank you
Bill
2019-07-22 10:30 PM
Hi Bill,
One point calibration can be applied to remove the residual offsets after soldering.
It is described in AN4833, Measuring pressure data from ST's LPS22HB digital pressure sensor,
section 4 Offset compensation.
After soldering, the measured offset can be stored in the RPDS (18h, 19h) registers and automatically subtracted from the pressure output registers: the output pressure register PRESS_OUT (28h, 29h and 2Ah) is provided as the difference between the measured pressure and the content of the register 256*RPDS (18h, 19h) (DIFF_EN = ‘0’, AUTOZERO =‘0’, AUTORIFP= ‘0’).
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.