2021-07-26 1:44 AM
Hi!
I'm having trouble to get FIFO to work. Registers write fine, but i think that OVRN flag never sets high.
My config:
CTRL_REG4, 0b01100111 //ODR = 100Hz, BDU = 0, ZYX enabled
CTRL_REG1, 0x00
CTRL_REG2, 0x00
CTRL_REG3, 0b00001000); //Interrupt signals active LOW, Interrupt signal latched, INT1 signal enabled
CTRL_REG5, 0b00000000); //BW = 00 anti aliasing 800Hz, Scale +- 2g, Self test disabled, SPI 4 wire
CTRL_REG6, 0b01000010); //FIFO enable, P1_OVERRUN enable (Interrupt on INT1 from OVERRUN flag)
FIFO_CTRL, 0b01000000); //Stream mode
And my interrupt routine:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){
if(GPIO_Pin == INT1_Pin){
for(int i = 0; i < 32; i++){
//X
outx_l = LIS3DSH_Read(OUT_X_L);
outx_h = LIS3DSH_Read(OUT_X_H);
outx = ( outx_h << 8 ) | outx_l;
//Y
outy_l = LIS3DSH_Read(OUT_Y_L);
outy_h = LIS3DSH_Read(OUT_Y_H);
outy = ( outy_h << 8 ) | outy_l;
//Z
outz_l = LIS3DSH_Read(OUT_Z_L);
outz_h = LIS3DSH_Read(OUT_Z_H);
outz = ( outz_h << 8 ) | outz_l;
}
}
}Normal mode, and DRDY mode with INT1 interrupt works fine. I think that FIFO never starts filling, when I read FIFO_SRC there is always EMPTY flag high.
I'm using STM32 F407 DISC board.
Thanks for help :)
2021-07-27 8:52 AM
Hi, did you compared your configuration with the one available for example on Github --> lis3dsh_fifo_stream.c
Especially the function lis3dsh_fifo_stream(void)
/* Set bdu and if_inc recommended for driver usage */
lis3dsh_init_set(&dev_ctx, LIS3DSH_DRV_RDY);
/* Select bus interface */
bus_mode = LIS3DSH_SEL_BY_HW;
lis3dsh_bus_mode_set(&dev_ctx, &bus_mode);
/* FIFO configuration */
lis3dsh_read_reg(&dev_ctx, LIS3DSH_FIFO_CTRL, ®.byte, 1);
reg.fifo_ctrl.fmode = 0x02; /* FIFO stream mode */
lis3dsh_write_reg(&dev_ctx, LIS3DSH_FIFO_CTRL, ®.byte, 1);
lis3dsh_read_reg(&dev_ctx, LIS3DSH_CTRL_REG6, ®.byte, 1);
reg.ctrl_reg6.fifo_en = PROPERTY_ENABLE;
lis3dsh_write_reg(&dev_ctx, LIS3DSH_CTRL_REG6, ®.byte, 1);
/* Configure interrupt pins */
lis3dsh_interrupt_mode_get(&dev_ctx, &int_mode);
int_mode.latched = PROPERTY_DISABLE;
lis3dsh_interrupt_mode_set(&dev_ctx, &int_mode);
lis3dsh_pin_int1_route_get(&dev_ctx, &int1_route);
int1_route.fifo_full =
PROPERTY_ENABLE; /* Enable hardware notification */
lis3dsh_pin_int1_route_set(&dev_ctx, &int1_route);
/* Set Output Data Rate */
lis3dsh_mode_get(&dev_ctx, &md);
md.fs = LIS3DSH_4g;
md.odr = LIS3DSH_800Hz;
lis3dsh_mode_set(&dev_ctx, &md);Tom
2021-07-27 10:27 PM
Thanks, I haven't found it before.
As far as I understand this code I did configuration mostly the same.
Maybe you worked on config yourself also?
2021-07-30 1:27 AM
I worked with this code and it did work
Did you configured the THRS3 (1Fh) overrun threshold for overrun detection?
Tom
2021-07-30 2:31 AM
Actually no, i didn't. What value it should contain in order to detect full FIFO? 0xFF?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.