2018-03-18 1:35 PM
I am using a LIS3DH to measure a machine's vibration, I understand that mems accelerometers are not usually used for this application, but nevertheless, I set up the acc to High resolution mode which gives me a bandwidth of 150Hz. I have the LIS3DH set up and comparing its data with a piezo accelerometer that I have. I noticed that at low frequency (under 40Hz) peak to peak values of both accelerometers are very similar. but when I go over that (80-100 Hz) I start to see a drop in the LIS3DH p-p compared to the other one. Is the LIS3DH just not suitable for this application ?
#lis3dh-machine2018-03-19 7:04 AM
What is the difference between the LIS3DH and the piezo sensor?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.