2018-03-15 9:24 AM
Hello,
Do you have any information about Vibration Rectification Error (VRE) on the LIS344ALH (2g setting)?
Specifically, I am driving the device into saturation. During and following the saturation, I am seeing what appears to be a significant DC offset on the output. This offset eventually decays, as long as the device is not forced back into saturation.
Has the behavior of the device been characterized when it enters saturation, especially if saturation is asymmetric in the presence of gravity?
Thanks,
Damon
2018-03-19 7:03 AM
We do not measure this characteristic.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.