2017-04-06 11:14 PM
I'm using the LIS3DH set at 1 Hz ODR. My SPI hardware seems to be working since DATA_RDY interrupts come in fine at a steady 1 second interval and the accelerometer data looks good. In fact I get good data at all speeds. However I can't seem to get the threshold interrupts working. I read the app notes, found setups on the web, and tried a lot of different configurations. Below is a sample setup.
Could you send me a register sequence that you know works to trigger an INT1 interrupt?
Also the ADC seems to give me 2032 to -2032 for a range of .9 to 1.8 volts maybe this is a clue. The temperature gives me -16 so I haven't been able to get this working either. Self test seems ok.
Thanks
Jeffrey Wedekind
#define LIS3DH_CONFIG_CTRL_REG1 0x17 // 1 Hz, Zen, Yen, Xen
#define LIS3DH_CONFIG_CTRL_REG2 0x00 // Default Settings #define LIS3DH_CONFIG_CTRL_REG3 0x40 // #define LIS3DH_CONFIG_CTRL_REG4 0x80 // #define LIS3DH_CONFIG_CTRL_REG5 0x00 // #define LIS3DH_CONFIG_CTRL_REG6 0x00 // #define LIS3DH_CONFIG_REFERENCE 0x00 // #define LIS3DH_CONFIG_INT1_CFG 0x95 // #define LIS3DH_CONFIG_INT1_THS 0x01 // #define LIS3DH_CONFIG_INT1_DURATION 0x01 // nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG1_rw, LIS3DH_CONFIG_CTRL_REG1); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG2_rw, LIS3DH_CONFIG_CTRL_REG2); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG3_rw, LIS3DH_CONFIG_CTRL_REG3); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG4_rw, LIS3DH_CONFIG_CTRL_REG4); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG5_rw, LIS3DH_CONFIG_CTRL_REG5); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_CTRL_REG6_rw, LIS3DH_CONFIG_CTRL_REG6);nrf51_tag_spi0_lis3dh_set_register(LIS3DH_INT1_THS_rw, LIS3DH_CONFIG_INT1_THS);
nrf51_tag_spi0_lis3dh_set_register(LIS3DH_INT1_DURATION_rw, LIS3DH_CONFIG_INT1_DURATION); nrf51_tag_spi0_lis3dh_set_register(LIS3DH_INT1_CFG_rw, LIS3DH_CONFIG_INT1_CFG);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.