2014-11-16 2:55 PM
I am unable to detect an interial interrupt from the LIS3DH accelerometer as a result of moving the sensor on a flat surface. The sensor is interfaced with an Arduino Uno using I2C. I am using the example in section 6.3.1 of AN3308, LIS3DH application notes. I can successfully read acceleration values. I also tried checking both interrupt ports, int 1 and int 2.
Please see attached Arduino code below.&sharpinclude <Wire.h>const int LIS3DH_ADDR = 0x18;int pin = 13;int int1Pin = 2;int int2Pin = 3;/* I2C Communication Set-up ---------------------------------------------------------*/unsigned int readRegister(byte reg) { Wire.beginTransmission(LIS3DH_ADDR); Wire.write(reg); Wire.endTransmission(); Wire.requestFrom(LIS3DH_ADDR, 1); return Wire.read();}void writeRegister(byte reg, byte data) { Wire.beginTransmission(LIS3DH_ADDR); Wire.write(reg); Wire.write(data); Wire.endTransmission();}/* Initialize accelerometer in the host processor. ----------------------------------*///It only needs to be executed one time after power up in initialization routine.void init_ACC(void){ // configurations for control registers writeRegister(0x20, 0xA7); //Write A7h into CTRL_REG1; // Turn on the sensor with ODR = 100Hz normal mode. writeRegister(0x21, 0x00); //Write 00h into CTRL_REG2; // High-pass filter (HPF) disabled writeRegister(0x22, 0x40); //Write 40h into CTRL_REG3; // ACC AOI1 interrupt signal is routed to INT1 pin. writeRegister(0x23, 0x00); //Write 00h into CTRL_REG4; // Full Scale = +/-2 g writeRegister(0x24, 0x00); //Write 00h into CTRL_REG5; // Default value. Interrupt signals on INT1 pin is not latched. //Users don�t need to read the INT1_SRC register to clear the interrupt signal. // configurations for wakeup and motionless detection writeRegister(0x32, 0x10); //Write 10h into INT1_THS; // Threshold (THS) = 16LSBs * 15.625mg/LSB = 250mg. writeRegister(0x33, 0x00); //Write 33h into INT1_DURATION; // Duration = 1LSBs * (1/10Hz) = 0.1s. writeRegister(0x30, 0x0A); //Write 0Ah into INT1_CFG; // Enable XLIE, YLIE interrupt generation, OR logic. }void setup() { Wire.begin(); Serial.begin(9600); int res = readRegister(0x0F); //WHO_AM_I Serial.println(res); pinMode(pin, OUTPUT); // sets the digital pin 13 as output pinMode(int1Pin, INPUT); // sets the digital pin 2 as input pinMode(int2Pin, INPUT); // sets the digital pin 2 as input}void loop() { //Read both interrupt pins int int1 = digitalRead(int1Pin); int int2 = digitalRead(int2Pin); Serial.print(int1); Serial.print('',''); Serial.println(int2); if (digitalRead(int1Pin) == 0 && digitalRead(int2Pin) == 0){ //if both are low write writeRegister(0x30, 0x0A); } else { digitalWrite(pin, HIGH); int intEvent = readRegister(0x31); Serial.println(intEvent); delay(2000); } delay(0);} #lis3dh-interrupt #accelerometer #lis3dh #lis3dh-interrupt2015-03-02 1:25 AM
I am be able to read out the x y z raw data from the acc lis3dh.
But I it can not generate INT signal. There is my configuration of the acc. LIS3DH_WriteReg(LIS3DH_CTRL_REG1,0x27); LIS3DH_WriteReg(LIS3DH_CTRL_REG2,0x01); // Interrupt driven to INT1 pad, AOI1 interrupt on INT1. ---0100 LIS3DH_WriteReg(LIS3DH_CTRL_REG3,0x40); // FS = 2g Full scale selection LIS3DH_WriteReg(LIS3DH_CTRL_REG4,0x00); // Disable FIFO temporarily; 0: interrupt request not latched;---0x00 //latched 0000 1000 ---0x08 LIS3DH_WriteReg(LIS3DH_CTRL_REG5,0x08); LIS3DH_WriteReg(LIS3DH_INT1_THS,0x08); // 0010 1010 beyond thresh hold ; 0001 0101 below thresh hold. event LIS3DH_WriteReg(LIS3DH_INT1_CFG,0x2a); uint8 val; LIS3DH_ReadReg(0x31, &val); //INT1_SRC------When I shake the acc, it just not generate INT signal , INT1 pin is low.2015-03-03 1:21 AM
Problem Found.
!!! without the delays between I2C operations, ACC is not configured correctly!!!Add delays. It works. MCU is Dialog M0.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.