2014-03-25 2:50 PM
The data sheet makes no explicit mention of a way to force this interrupt to latch and clear when the CLICK_SRC register is read (like the INT1_CFG registers can).
App note AN3308 states that this behavior can be achieved by setting the LIR bit in the TAP_CFG register. However, this bit is not documented in the data sheet. Another, similar part perhaps? I'm seeing the interrupt hold for the duration of the CLICK_LATENCY period as expected but would like to clear this sooner as I'm using the data ready signal on the same line. Is there anything I can do to accomplish this? I'm sampling at a fairly low data rate (10hz) so shortening the latency period is not an option. I am using an OEM board that does not have INT2 hooked up. #li3dh-click2014-07-15 7:42 AM
Any updates on this ? I am having the same problem. The click activates the external interrupt line, but reading CLICK_SRC register doesn't give any information on the source of the interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.