2019-07-01 12:14 AM
I am attempting to get a double click interupt working on the LIS3DH. I have been using the INT1 pin for regular threshold interrupt but have another application which requires the click interrupt.
So far, after playing with many thresholds and timing - I cannot get any combination to actually register a click/double clock. Can anyone who has succuesfully gotten doubleclick to work please share there configuration. (Even adafruit library seems ineffective)
2019-07-01 4:07 AM
Hi @Community member are you using ODR 400Hz or high, right? This is important to be able to detect a rapid event such as a click. Did you also followed all the indication of the AN3308 app note (p 32-37, DCLICK in CLICK_SRC correctly enabled etc)? You could share your code or an oscilloscope screen of INT1 working. Regards
2019-07-04 6:17 PM
Hi Eleon,
Thanks for the prompt response, the 400hz refresh rate was what was holding me back- i have this working succesfully now thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.