2013-11-11 7:12 PM
I have used the LIS3DH for movement and angle detection for about 18 months. I now wish to use it for fall detection. Previously I ued another brand where you setup a register and get an interrupt when a zero G occurs in all axes for a certain time. I can see no way to do this with the LIS3DH but it advertises that it can be done. I can do it ''manually'' by continually reading each axis and setting a timer to record when it is continuously like this for, say 100mS. Is there an easier way that uses less power?
Thanks2013-11-11 7:51 PM
Hello Peter.
May be ''Application Note'' AN3308 is help you?CD00290365.pdf: AN3308, 6.3 Free-fall and wake-up interrupts:The LIS3DH interrupts signal can behave as free-fall and wake-up. (and so on...)2013-11-18 5:24 AM
Hello Peter and Gav,
In order to support your free fall application development I have attached an image showing a suggestion for the registers setup of the LIS3DH for a free fall interrupt in low power mode. I have also attached the LIS3DH datasheet where you will be able to find a better description of each register. Thank you very much, Thiago Reis ________________ Attachments : LIS3DH_FREE-FALL.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzKD&d=%2Fa%2F0X0000000bKD%2FNMbOBN.L9xyAL5MAg_jKSF2AVHKZ7VfkUbRJLaebc.U&asPdf=falseLIS3DH.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzL5&d=%2Fa%2F0X0000000bKF%2FK7hzlEqd6e8MgzzRWeCvKFMgD3KPwHpnd.0ponF5f7o&asPdf=false2015-12-29 4:27 AM
It appears that some of the registers in the attached image from Thiago Reis (e.g. INT2_CFG, INT2_THS) are not defined in the datasheet. Also, I'm not able to see an interrupt when executing the sequence in paragh. 6.3.3 of AN3308 (Wakeup with HPF). I was not able to find the address of the register HP_FILTER_RESET mentioned in step # 8, since this register is also missing from the datasheet. Could there be an updated version of the datasheet that I may have missed? It would be great if someone at ST could send a working sequence for the wake-up usecase with HPF turned on.
Thanks,2016-03-29 3:29 AM
Confirm some registers aeems to be marked as reserved with a threatening note stating not to modify them or damage will happen.
Is this some kind of mistake?StefanoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.