2018-05-17 3:06 AM
Hello,
I
checked the lis3dh manual, there is such a sentence “
The status of the 321DA bit can be driven to the INT1 pad by setting the I1_DRY2 bit of CTRL_REG3 to 1.� ,I have do it(ADC_PD bit of TEMP_CFG_REG (1Fh) to 1,
ODR bit of CTRL_REG1(20h) to 1HZ ), but can’t get interruptes signals.INT1 pin is always high. other work well.
Thanks for your help.
2018-05-22 12:08 PM
Can you share you complete sensor configuration so I can check it?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.