cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH: 12 Bit Resolution and FIFO Mode

Aaron Derbyshire
Associate II
Posted on November 30, 2017 at 11:19

Given that the LIS3DH FIFO is only 10 bit wide, is it actually possible to run the accelerometer with 12 bit resolution?

#12-bit #lis3dh #fifo
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on December 01, 2017 at 17:40

I think if the sensor is configured int Low-power mode (8-bit resolution) also only 8-bit value is stored in the FIFO (the low bytes are 0).

View solution in original post

4 REPLIES 4
Miroslav BATEK
ST Employee
Posted on November 30, 2017 at 16:09

If FIFO is disabled and the sensor is configured into High-resolution mode the output is 12-bit.

0690X0000060925QAA.png
Posted on November 30, 2017 at 16:21

As I anticipated, thank you.

Does this mean that similarly if I have the sensor configured into a FIFO mode with 8 bit resolution I will still achieve 8 bit resolution?

Posted on December 01, 2017 at 17:40

I think if the sensor is configured int Low-power mode (8-bit resolution) also only 8-bit value is stored in the FIFO (the low bytes are 0).

Posted on December 01, 2017 at 17:51

Thanks, I thought this may be the case but just wanted to double check as it's not specified in the datasheet or in AN3308.

Thanks again!
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.