cancel
Showing results for 
Search instead for 
Did you mean: 

lis302dl on STM32f407 VG Y Axis do not Change

yasinbjk50
Associate III

Hello,

I have been trying to make a accelerator project by using lis302dl accelorator on STM32f407 vg discovery card. There are three axis which are x, y and z. These have x, y and z variables according to position of lis302dl on the card. I have used SPI1 and E3 pin for CS. When ı observe the values on STM Studio, x and z variables changed everytime which is good. However y variables is always zero, I enabled x, y, z on lis302 dl register though. Can somebody give me idea about what I am doing wrong?

 

 

 

#include "stm32f4xx.h"
#include "stm32f4_discovery.h"

GPIO_InitTypeDef GPIO_InitStruct;
SPI_InitTypeDef SPI_InitStruct;

uint8_t x,y,z;
uint8_t x_address = 0x29, y_address = 0x2B, z_address = 0x2D, m_data = 0x00;

void GPIO_Config()
{

	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

	GPIO_InitStruct.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;
	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_Init(GPIOD, &GPIO_InitStruct);

	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);	// for CS pin

	GPIO_InitStruct.GPIO_Mode=GPIO_Mode_OUT;
	GPIO_InitStruct.GPIO_Pin=GPIO_Pin_3;
	GPIO_InitStruct.GPIO_OType=GPIO_OType_PP;			//
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;		//
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_Init(GPIOE, &GPIO_InitStruct);


	RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

	GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);	// SCK pin
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);	// MOSI pin
	GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);	// MISO pin

	GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;
	GPIO_InitStruct.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;
	GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;	//
	GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;	//
	GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
	GPIO_Init(GPIOA, &GPIO_InitStruct);
}

void SPI_Config()
{
	RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);

	SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
	SPI_InitStruct.SPI_CPHA = SPI_CPHA_2Edge;
	SPI_InitStruct.SPI_CPOL = SPI_CPOL_High;
	SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b;
	SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
	SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
	SPI_InitStruct.SPI_Mode = SPI_Mode_Master;
	SPI_InitStruct.SPI_NSS = SPI_NSS_Soft|SPI_NSSInternalSoft_Set;

	SPI_Init(SPI1, &SPI_InitStruct);

	SPI_Cmd(SPI1, ENABLE);

	GPIO_SetBits(GPIOE, GPIO_Pin_3);	// CS pin locig 1
}

void SPI_Write(uint8_t address, uint8_t data)
{
	GPIO_ResetBits(GPIOE,GPIO_Pin_3);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE));

	SPI_I2S_SendData(SPI1,address);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_RXNE));

	SPI_I2S_ReceiveData(SPI1);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE));

	SPI_I2S_SendData(SPI1,data);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_RXNE));

	SPI_I2S_ReceiveData(SPI1);

	GPIO_SetBits(GPIOE,GPIO_Pin_3);

}

uint8_t SPI_Read(uint8_t address, uint8_t data)
{
	GPIO_ResetBits(GPIOE,GPIO_Pin_3);

	address = address | 0x80;

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE));

	SPI_I2S_SendData(SPI1,address);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_RXNE));

	SPI_I2S_ReceiveData(SPI1);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE));

	SPI_I2S_SendData(SPI1,data);

	while(!SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_RXNE));

	SPI_I2S_ReceiveData(SPI1);

	return SPI_I2S_ReceiveData(SPI1);

}

void delay(uint32_t time)
{
	while(time--);
}

int main(void)
{
  GPIO_Config();
  SPI_Config();
  SPI_Write(0x20,0x67);

  while (1)
  {
	  x = SPI_Read(x_address, 0x00);
	  y = SPI_Read(y_address, 0x00);
	  z = SPI_Read(z_address, 0x00);

	  delay(20);
  }
}

void EVAL_AUDIO_TransferComplete_CallBack(uint32_t pBuffer, uint32_t Size)
{
  return;
}

uint16_t EVAL_AUDIO_GetSampleCallBack(void)
{
  return -1;
}

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.