cancel
Showing results for 
Search instead for 
Did you mean: 

FP-SNS-DATALOG1 DeviceConfig.json

TomRett
Associate III

Can i reduce the sensitivity ("sensitivity": 1) for a microphone (IMP23ABSU) for it not to reach the 130dbSPL?

What does the "samplesPerTs": 1000" translate to?

Is the sampling frequency defined with "ODR": 192000" or "ODRMeasured": 192000" ? What is the connection and the difference between ODR and ODRMeasured?

 

TomRett_1-1699733239524.png

That is the reason i want to achieve the reduction of sensitivity. Im measuring an air-leakage that has a diameter or 1 mm at a distance of 20 cm. The Amplitudes are normalized (x * 1V/32768). Any ideas on how to achieve this?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.