2017-04-02 4:10 PM
I have LIS2HH12TR on a PCB. I want to implement Tap Detection. I could not find a direct Register for configuring Interrupt for a tap. It would be great to refer to Example code for Tap Detection using Raw Accelerometer Data or any other alternative method using LIS2HH12TR?
#accelerometer #lis2hh12 #tap2017-04-04 9:01 AM
Unfortunately LIS2HH12 doesn't have build in click/double-click recognition feature.
You would have to detect in by software.
2019-01-02 9:50 PM
The question: "... It would be great to refer to Example code for Tap Detection..."
This would be the software you are referring to.
Can someone provide example software, consisting of at least some device settings? Otherwise, one might conclude that it is difficult to implement.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.