2023-04-30 8:39 PM
I am using LIS2DH to detect the tilt angle of a vessel. Sometimes the XYZ reading will freeze, and not update anymore, the only way to reset it is to power on/off the system.
2023-05-02 7:48 AM
Hi @che.1 ,
Welcome to ST Community!
Can you give me more details? For example, which are your settings? Are you in SPI or I2C mode?
2023-05-08 2:57 PM
The setting for register 0x20 is 0x27,others is default. I am using I2C to read the XYZ since it only detects tilt, so only Z is continuously monitored. Sometimes it will stuck at 960 for the z-axis, will reset 0x20 help?
2023-05-10 2:56 AM
Hi @che.1 ,
does it happen always after a certain amount of time or is it random?
by freezing do you mean that it always returns the same value continuously or it does not return anything anymore?
can you read the CTRL_reg1 (20h) and CTRL_REG4 (23h) when it happens?
Niccolò
2023-05-11 9:32 AM
it’s very difficult to recreate the problem. I have 2 broken PCBAs that I have been trying to recreate the problem with for 2 weeks and I haven’t been successful. Once it’s frozen at 960, it never changes until we do a hard reset. (unplug the battery)
2023-05-22 5:54 AM
I'm sorry, but I'm not able to replicate the issue, so without further info from your side, I don't know how to help you.
the only other thing it can be checked is if the FIFO is full and you are not dumping it, but having default settings it should not be the case.
Let me know if you have any more updates =)
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.