2017-11-11 11:35 PM
Hi, I'm working with LIS2DE12 for motion detection. I have configured INT1. Whenever motion is detected I'm reading INT1_SRC but its value is not changing. It is always same 01101000. Here's the configurations I have set.
CNTRL_REG0 = 10h //SDO pull_up connected
CNTRL_REG1 = 3Fh //25Hz, Enable XYZ axes
CNTRL_REG2= 03h //HPF enabled for Interrupt
CNTRL_REG3= 40h //INT1 on INT1 pin
CNTRL_REG4 =00h //Default BDU disabled
CNTRL_REG5= 04h //4D enabled
CNTRL_REG6= 20h // INT2 Interrupt on INT2 pin /clk INT2 & activity INT DISABLED..
INT1_CFG = 7Fh //X,Y,Z interrupts , 6-D enabled
INT1_THS = 05h
INT1_DUR = 03h // (03/25) seconds.
Also OUT_X_H, OUT_Y_H, and OUT_Z_H gives always same values. Anything I'm missing in the configuration? help me out of this.
#accelerometerSolved! Go to Solution.
2017-11-14 9:18 AM
I got it working by setting FIFO register settings correctly. But in datasheet it is told to read acceleration data with starting address 28h.. But with that address if read 6-bytes upto 2Dh it is giving always zeros.. If the starting address for acc_data reading is given as (08h | 28h) instead of 28h acc_data values are reading correctly. Then I'm able to read x,y,z acc_data ..Why it is like that.?
2017-11-14 9:18 AM
I got it working by setting FIFO register settings correctly. But in datasheet it is told to read acceleration data with starting address 28h.. But with that address if read 6-bytes upto 2Dh it is giving always zeros.. If the starting address for acc_data reading is given as (08h | 28h) instead of 28h acc_data values are reading correctly. Then I'm able to read x,y,z acc_data ..Why it is like that.?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.