2018-01-07 11:08 PM
Hi, I am working on a custom board wherein, I am using LIS2DE12 accelerometer. The custom board draws around 0.1mA current. After the removal of the accelerometer from the board, the board drwas only 3uA current. So, I would like to disable the accelerometer operation for minimising the current consumption, and for this, after initialization, I am writing the power down command 0x00 to the register CTRL_REG1 (20h). But the accelerometer still draws 0.1-0.2mA current. Please suggest the possible reasons for the same.
Thanks
#lis2de12 #accelerometer2018-01-08 7:40 AM
I suppose you connected the SA0 pin to GND and the current is drawn by this pin, because this pin has internal pull-up.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.