2022-05-24 4:48 PM
I have downloaded all the needed software and st-link (and update) but Unicleo_GUI does not recognize the expansion board. In my device manager, the virtual COM is there. I am able to connect to the right port, but only if I tick the box that lists all the COM ports. Any help is much appreciated. Thanks
Solved! Go to Solution.
2022-05-26 7:17 AM
Hello @DLlam.1 and welcome to the Community :)
The X-NUCLEO-IKS01A3 is compatible with Nucleo-L552ZE-Q (with STM32 Nucleo boards)
Maybe you have to check solder bridges.
You can check if the available -ready to use- examples with STM32L5 are working.
Make sure to include the IKS01A3 from the BSP folder under X-CUBE-MEMS package:
STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\8.3.0\Drivers\BSP
and Import the Components folder from X-CUBE-MEMS package: STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\9.2.0\Drivers\BSP\Components
then, add it in the Components folder of the CubeL5 package:
STM32Cube\Repository\STM32Cube_FW_L5_V1.4.0\Drivers\BSP\Components
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2022-05-26 7:17 AM
Hello @DLlam.1 and welcome to the Community :)
The X-NUCLEO-IKS01A3 is compatible with Nucleo-L552ZE-Q (with STM32 Nucleo boards)
Maybe you have to check solder bridges.
You can check if the available -ready to use- examples with STM32L5 are working.
Make sure to include the IKS01A3 from the BSP folder under X-CUBE-MEMS package:
STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\8.3.0\Drivers\BSP
and Import the Components folder from X-CUBE-MEMS package: STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-MEMS1\9.2.0\Drivers\BSP\Components
then, add it in the Components folder of the CubeL5 package:
STM32Cube\Repository\STM32Cube_FW_L5_V1.4.0\Drivers\BSP\Components
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.