2017-02-22 5:39 PM
Hi, I have a project that uses LIS3DH. I just noticed an update at the Datasheet and now there is a CTRL_REG0 that I can disable the SA0 pull-up. Is this available since the beginning or just on new batches of the device?
2017-02-23 12:14 AM
It is available since the beginning.
2017-04-25 12:51 PM
Thank you. Is there any special procedure or timig restriction to disable the pull-up? I am using the LIS3DH with the SPI and i see some current leakage with the pull-up? Sometimes i send the command and the current goes away and sometimes it dont.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.