2020-09-01 5:55 AM
Hello
I have advanced in my tests and in the realization of my product via the st APIs for the VL6180X, I need to carry out an interrupt during the detection of the target (my hand), I set my interrupt thresholds with sample_interrupt.c, however I want to run the LED with a Timer to indicate the interrupt time. Which file should be modified to achieve this? If you have any other information that might help me, we are interested. Thank you.
Regards,
Myveck
2020-09-03 7:29 AM
I'm not exactly sure what your are asking, but I'll give it a shot.
In my code, I'm asleep at a point - waiting for interrupt.
This is a built-in function. There should be something similar in your code.
#define __WFI __iar_builtin_WFI
When the interrupt comes in, read the distance data.
Then it's a matter of raising the GPIO pin attached to your LED.
On an STM32, you configure your GPIO, and you can raise and lower it at will.
Google "stm32 gpio tutorial" it will get you to some good information
If you want to use a timer to time the time between interrupts,
Google "STM32 HAL_GetTick()" it returns the number of milliseconds elapsed since startup.
So you can measure the time between calls.
2020-09-03 9:11 AM
Ok thank you John,
I translate from French to English that's why there is this concern.
I understood your explanation, I am using the sample interrupt function to create my user program. I would like to know how I can do to turn on the green LED of the Nucleo STM32 when the sensor detects the target and I want it to turn off when there is no target.
thank you so much
2020-09-11 5:23 AM
Hi @MSAMB.1 ;
is your last question here above related to this thread?
If so, can you please check if Nizar's answer can be of any help for you?
Tks
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.