2017-11-02 6:39 AM
Hi All
i will use 'L3GD20H MEMS motion sensor: three-axis digital output gyroscope' in my Project.
Pin No 7. which is INT1(Programmable interrupt).
Please share me how its pin work. when its generate interrupt.
Thanks!
#gyro-lsm330dl #mems-gy #l3gd20h #mems #gyroscopes #a3g4250d-mems-gyro #l3g4200d-gyroscope #gyroscope2017-11-05 12:26 PM
Please check the
especialy description of register CTRL3, where you can setup the funtionality of interupt pins.Then you should check chapter 7.15 - 7.20 where you can find configuration of the interrupt generator for INT1. Basicaly the interrupt can be generated if the output value is below or above a certain treshold.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.