2022-06-08 5:58 AM
I'm trying to interface with the LSM303AGR using the 3-wire SPI protocol. I'm polling the registers 0x28 - 0x2D in high-accuracy mode, and what I've noticed is that the least-significant nibble of each axis is occasionally 0x1 instead of 0x0 as expected. I understand that the data needs to be right shifted by one nibble, but I would've expected the least significant nibble to always be 0x0 if the data is 12-bit left-justified. Does this last bit have any significance?
Example data (Queried with 0xE8):
X LSB X MSB Y LSB Y MSB Z LSB Z MSB
0x00 0xFE 0x20 0x20 0xC1 0x1A
0x00 0xEF 0x61 0x2F 0x 21 0x9C
0xC1 0xC9 0x41 0xF0 0x61 0x8B
2022-06-10 7:34 AM
Hi @ESun.1 ,
I would agree with you, the last 4 bits should be all 0.
Did you try to convert a stream of data in physical units and see if you are getting sensible values (e.g. 1g along z axis, and almost 0g along the others when the device is in steady condition)?
float_t lsm303agr_from_fs_2g_hr_to_mg(int16_t lsb)
{
return ((float_t)lsb / 16.0f) * 0.98f;
}-Eleon
2022-12-26 9:33 PM
Hi @ESun.1 . How do you communicate with 3 wire SPI ? I cant communicate. How did you connet the hardware ? What did you choose SPI mode. Full Duplex or half duplex ? Can you help me ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.