2022-08-24 2:22 PM
Solved! Go to Solution.
2022-08-24 2:41 PM
1101010x for SA0=0 (0x6A << 1)
1101011x for SA0=1 (0x6B << 1)
2022-08-24 2:41 PM
1101010x for SA0=0 (0x6A << 1)
1101011x for SA0=1 (0x6B << 1)
2022-08-24 2:55 PM
Thank you, did I miss this in the datasheet?
2022-08-24 3:13 PM
The low order bit was mentioned several times, the actual address pattern wasn't, even in things like the timing diagram
https://github.com/STMicroelectronics/iis3dwb-pid/blob/master/iis3dwb_reg.h
@Amel NASRI can we flag the data sheet issue to the technical writers, thanks
2022-08-25 1:22 AM
Hi @Community member ,
I let @Eleon BORLINI take care of this request.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-25 1:24 AM
Hi,
let me add that, for IIS3DWB, the SPI communication protocol is recommended, especially if the device is configured in 3-axis mode, since the ODR is fixed at 26.67kHz and is quite high for a sensor.
Anyway, I'll notify this missing info to our technical writers team.
-Eleon
2022-08-25 9:27 AM
Understood, playing devils advocate here.
Data sheet lacks detail on I2C speed supported too, so 400 KHz, or 1 MHz ?
A table of anticipated bandwidths may make the I2C vs SPI case more strongly.
I think @JLee had a different question/thread, where it's a sub-set of functionality, or triggering, that's desired.
https://www.st.com/resource/en/datasheet/iis3dwb.pdf
2022-08-25 5:44 PM
But as I mentioned in my other post and repeated here, I don't care about getting the data out at high sample rates. I'm just using the interrupts for thresholds and want to use this part because it has a higher bandwidth for detection.
In I2C mode for the IIS3DWB device the datasheet says it only support single axis mode because I2C is too slow to get the data. I want to use I2C mode to configure either wake up or activity thresholds for all 3 axis and then configure the interrupts to tell me those thresholds were exceeded. I don't need the data.
So the questions are In I2C mode:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.