2023-07-05 7:23 PM
Hi
I am using an IIS2DH accelerometer and set up FIFO. The configuration sequences are following the IIS2DH example in Github, see below
// 25Hz, Low-Power Mode Disabled, XYZ enabled
ACC_Write_Command(IIS_CTRL_REG1, IIS_CTRL_REG1_INIT_25HZ);
// High-Pass Filter on INT2, FIFO disabled, interrupt registers in latched mode
ACC_Write_Command(IIS_CTRL_REG2, IIS_CTRL_REG2_INIT);
// +/-2g (4g full scale), HR Enabled
ACC_Write_Command(IIS_CTRL_REG4, IIS_CTRL_REG4_INIT_2G);
// Stream buffering on the acc
ACC_Write_Command(IIS_FIFO_CTRL_REG, IIS_FIFO_CTRL_REG_INIT_STREAM);
// Enable FIFO for this type of Tag
ACC_Write_Command(IIS_CTRL_REG5, IIS_CTRL_REG5_INIT_FIFO);
However, the accelerometer data is not updating until I am adding a 5 ms delay after writing the Stream Mode to the register. See below,
// 25Hz, Low-Power Mode Disabled, XYZ enabled
ACC_Write_Command(IIS_CTRL_REG1, IIS_CTRL_REG1_INIT_25HZ);
// High-Pass Filter on INT2, FIFO disabled, interrupt registers in latched mode
ACC_Write_Command(IIS_CTRL_REG2, IIS_CTRL_REG2_INIT);
// +/-2g (4g full scale), HR Enabled
ACC_Write_Command(IIS_CTRL_REG4, IIS_CTRL_REG4_INIT_2G);
// Stream buffering on the acc
ACC_Write_Command(IIS_FIFO_CTRL_REG, IIS_FIFO_CTRL_REG_INIT_STREAM);
//introduce a 5ms delay to allow sufficient time for the sensor to update its registers with the latest data
delay_mSec(5);
// Enable FIFO for this type of Tag
ACC_Write_Command(IIS_CTRL_REG5, IIS_CTRL_REG5_INIT_FIFO);
I could not find any clue in the datasheet, we need a delay after certain FIFO mode registrations.
Could anyone help me check my configuration, and why do we need a delay in between writing registers.
Thanks.
2023-07-06 11:29 PM
Hi @cr_0trakka0 ,
Welcome to ST Community!
Have you already tried to enable Block Data Update (reg CTRL_REG4 (23h)), set the FIFO watermark and the FIFO mode to Stream mode?
2023-07-09 7:13 PM
Thanks for your reply.
I have the Block Data Update enabled, as it is set by default value ' 0 '.
Yes, I set the FIFO mode to Stream mode by "FIFO_CTRL_REG", however, I am not using the FIFO watermark, as in the application it is reading the accelerometer data instantly in a real-time way.
Currently, it is only working with adding some time delay (5-10ms) after setting the "FIFO_CTRL_REG", otherwise the accelerometer data is not updating, and is stuck at the beginning.
Thanks
2023-07-10 9:03 AM
Hi @cr_0trakka0 ,
what do you mean by "stuck"? is it static at 0?
could you check if the registers were written correctly immediately after writing them? (mainly IIS_FIFO_CTRL_REG and IIS_CTRL_REG5)
Niccolò
2023-07-10 9:58 PM
Hi @niccolò
Yes, all the accelerometer data is static at 0, and not updating.
I double check the register values that are correct. See code below
// 25Hz, Low-Power Mode Disabled, XYZ enabled
ACC_Write_Command(IIS_CTRL_REG1, IIS_CTRL_REG1_INIT_25HZ);
// High-Pass Filter on INT2, FIFO disabled, interrupt registers in latched mode
ACC_Write_Command(IIS_CTRL_REG2, IIS_CTRL_REG2_INIT);
// +/-2g (4g full scale), HR Enabled
ACC_Write_Command(IIS_CTRL_REG4, IIS_CTRL_REG4_INIT_2G);
// Stream buffering on the acc
ACC_Write_Command(IIS_FIFO_CTRL_REG, IIS_FIFO_CTRL_REG_INIT_STREAM);
// Enable FIFO for this type of Tag
ACC_Write_Command(IIS_CTRL_REG5, IIS_CTRL_REG5_INIT_FIFO);
The register written sequences are following the code example on Git https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/iis2dh_STdC/examples/iis2dh_fifo_read.c
The accelerometer will update data once I add a 5ms delay after writing the register "IIS_FIFO_CTRL_REG" for selecting Stream mode, is this the correct way to set up this accelerometer?
2023-07-11 1:57 AM
Hi @cr_0trakka0 ,
sorry, I didn't explain myself well, I suggested to read the register right after writing it, just to confirm that the ACC_Write_Command was performed correctly.
could you also perform the full operations of the example (set also BDU and watermark), just to confirm that everything is all right?
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.