2019-03-26 1:20 PM
Hi,
I can only seem to read 10bit resolution despite setting the following:
REG_CTRL1 = 0b00000111;
REG_CTRL4 = 0b00001000;
I have low power mode disabled and HR mode enabled, but the precision does not increase from Normal Mode.
Am I missing something?
2019-03-27 8:40 AM
Hi, it should work.. Could you share e.g. the OUT_X_L (28h) and OUT_X_H (29h) values? do you concatenate it in the right way? Please consider that the sens is 3.91 mg/digit for NM and for 0.98 mg/digit in case of HR mode
2019-03-27 9:54 AM
Here is the output of a resting module @ 2G / 25Hz ODR. I am reading values from the FIFO queue. I am triggering the read at the watermark level of 28.
High Res Mode
REG_CTRL1 = 0b00000111;
REG_CTRL4 = 0b00001000;
[98195] OUT_X_LH 00 80
[98214] OUT_X_LH 06 C0
[98236] OUT_X_LH 0C C0
[98257] OUT_X_LH 12 80
[98278] OUT_X_LH 18 C0
[98299] OUT_X_LH 1E 00
[98320] OUT_X_LH 24 00
[98342] OUT_X_LH 2A C0
[98363] OUT_X_LH 30 00
[98384] OUT_X_LH 36 00
[98405] OUT_X_LH 3C 00
[98426] OUT_X_LH 42 C0
[98448] OUT_X_LH 48 00
[98469] OUT_X_LH 4E C0
[98490] OUT_X_LH 54 00
[98511] OUT_X_LH 5A 00
[98532] OUT_X_LH 60 00
[98554] OUT_X_LH 66 C0
[98575] OUT_X_LH 6C 40
[98596] OUT_X_LH 72 00
[98617] OUT_X_LH 78 40
[98638] OUT_X_LH 7E 40
[98660] OUT_X_LH 84 00
[98681] OUT_X_LH 8A 00
[98702] OUT_X_LH 90 00
[98723] OUT_X_LH 96 C0
[98744] OUT_X_LH 9C C0
[98766] OUT_X_LH A2 00
Normal Mode
REG_CTRL1 = 0b00000111;
REG_CTRL4 = 0b00000000;
[58168] OUT_X_LH 00 C0
[58187] OUT_X_LH 06 40
[58209] OUT_X_LH 0C C0
[58230] OUT_X_LH 12 80
[58251] OUT_X_LH 18 40
[58272] OUT_X_LH 1E 80
[58293] OUT_X_LH 24 80
[58315] OUT_X_LH 2A 80
[58336] OUT_X_LH 30 40
[58357] OUT_X_LH 36 C0
[58378] OUT_X_LH 3C 40
[58399] OUT_X_LH 42 00
[58421] OUT_X_LH 48 00
[58442] OUT_X_LH 4E 80
[58463] OUT_X_LH 54 80
[58484] OUT_X_LH 5A 00
[58505] OUT_X_LH 60 00
[58526] OUT_X_LH 66 40
[58548] OUT_X_LH 6C 40
[58569] OUT_X_LH 72 00
[58590] OUT_X_LH 78 80
[58611] OUT_X_LH 7E 00
[58633] OUT_X_LH 84 C0
[58654] OUT_X_LH 8A 80
[58675] OUT_X_LH 90 C0
[58696] OUT_X_LH 96 40
[58717] OUT_X_LH 9C C0
[58739] OUT_X_LH A2 C0
Am I not converting correctly?
X = (int16_t)(i2c_read_data[i+1] << 8 | i2c_read_data[i]));
2019-03-28 8:04 AM
Let me put it another way...
In HR Mode I expect raw values to change by a factor of 16.
In Normal Mode I expect raw values to change by a factor of 64.
In LP Mode I expect raw values to change by a factor of 256.
What I observe is the following:
HR Mode: 64
Normal Mode: 64
LP Mode: 256
So, I am not seeing 12-bit or at least there does not appear to be a difference between HR and Normal modes.
2019-03-28 8:14 AM
So, now I see the issue. The FIFO only supports 10bit. Ugg.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.