2022-03-29 7:22 AM
LSM6DSOX Inertial module handles linear acceleration output data rate up to 6667 Hz, while limit for MLC and FSM is 104 Hz.
2022-03-31 8:58 AM
Hi @PTHOM.1 ,
unfortunately the limit of this ODR=104Hz cannot be overcome in the LSM6DSOX/RX family, since its clock/logic is shared also with the sensor hub, which can be synchronized with the accelerometer/gyroscope data-ready signal up to 104 Hz.
Next generation IMU sensors with ISPU, such as LSM6DSO16IS, will be capable of much higher ODRs (and more complex functions).
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.